*** Booting nRF Connect SDK v3.1.1-e2a97fe2578a ***
*** Using Zephyr OS v4.1.99-ff8f0c579eeb ***
[00:28:01.958,611] main: ========================================
[00:28:01.958,616] main: XIAO nRF54L15 SD Card Sample
[00:28:01.958,620] main: ========================================
[00:28:01.958,624] main: Checking SD card…
[00:28:01.958,633] main: Block count: 0
[00:28:01.958,641] main: Block size: 0 bytes
[00:28:01.958,646] main: Total size: 0 MB
[00:28:01.984,539] sd: Maximum SD clock is under 25MHz, using clock of 24000000Hz
[00:28:02.016,750] main: Filesystem mounted at /SD:
[00:28:02.075,279] main: Created test file: /SD:/test.txt
[00:28:02.075,733] main: SD card unmounted
[00:28:02.075,739] main: ========================================
[00:28:02.075,743] main: Sample completed
[00:28:02.075,748] main: ========================================
I can write data to it, but I can’t retrieve any information from my FAT32 SD card. Is there anything I can try?