Hello SeeedStudio Community,
I’m currently working on an STM32 project in STM32CubeIDE and need assistance integrating the Grove LED Matrix Driver (HT16K33) library for a Grove 8x8 LED matrix. I’ve downloaded the Grove_LED_Matrix_Driver_HT16K33 library, but I’m facing challenges getting it to work on the STM32 platform.
- I’ve placed the library files in the
Srcdirectory of my STM32 project. - Configured I2C in STM32CubeIDE, but I’m uncertain if I need to manually adjust the I2C address or do additional configurations for the STM32 to recognize the matrix on the bus.
- I tried including the main header file (
Grove_LED_Matrix_Driver_HT16K33.h) inmain.c, but I keep getting compilation errors, particularly withI2Cdev.h. It seems to be designed specifically for Arduino??, which is causing compatibility issues on the STM32 platform.
I am completely new to the microcontroller game. sorry if i sound stupid