Hi, I am new to the Wio Terminal and programming. I am trying to find a way to make the infrared emitter grove work on the Wio Terminal. Right now I have the raw infrared data ready but I do not know how I could emit it. I have tried some of the example sketches but they didn’t work for me. I connected the grove infrared emitter to the Wio Terminal via the 4-pin grove wire but I do not know what pin I should use.
Hi good_groups
Actually, the wio terminal comes with its own Infrared emitter, so you don’t need to connect an additional Infrared emitter. For details on how to use the built-in Infrared emitter, please see this wiki article
Hello.
It’s very ok WIO terminal have own IR emiter. It work fine.
But… if i use it with battery case, a battery case covers default IR emiter.
How to change my program to choose extrernal IR emiter ? ( D0, D4, etc) Via WIO_IR ?
if You need use extrenal IR Emiter with WIO Terminal ( f.e. battery chassis cover IR emiter) via Seeed_Arduino_IR repositorie edit file IRLibSAMD51.h line:
#define IR_SEND_PWM_PIN WIO_IR
to:
#define IR_SEND_PWM_PIN 0 // WIO_IR (for D0) pin
I need to get me one of these too, thanks for reminding me