Infrared Emitter and Receiver as a BEAM

Hello there, i’m new to this forum. Sorry for my bad english. I write here because i need help for a project of mine. I want to use the two sensors i wrote in the subject to create a “beam” that can be interrupted when something pass between them. Is this possible with those two sensors? I want arduino to notice when something or someone interrupt the beam and make him do something!

Hello,

Yes it is possible with the following sensors

1.Grove-Infrared Receiver
2.Grove Infrared Transmitter
and the example code is available in the wiki
documentation.

Please also check the Grove IR distance interrupter which has both transmitter and receiver in it.