I believe the erase and upload steps are both essential to make the firmware update occur, after copying the uf2 file. Both of those additional steps must complete as specified in the instructions. Once those steps are taken, double click the reset button. Then you can and should ignore the fact that the screen still shows “Burn fw mode”. That part only changes once a new sketch is uploaded.
1 Like