I would like to connect a IMU to the Odyssey-X86i51135G7 for real-time measurements. For example, using something like a 6 DOF IMU connected through i2C. I’m not sure if it is possible, as I can not find the exact datasheet and/or pin layout of the Odyssey-X86i51135G7.
Thus, I would like to know the pin layout for this patform. I saw on the forum that the ReServer uses this board inside, but I could not find the pin layout. And I could not find the information on seeedstudio. com either.
Thank you for the answer. Unfortunately, I can not find the information about the pins in the description of the ReServer (28-pin Arduino Pinout, 9-pin COM Pinnoutx2, 9-pin USB2.0 Pinout, 9-Pin Front panel Pinout, see https://files.seeedstudio.com/wiki/reServer/wiki/reServer%20mainboard%20.png). Is there anywhere a description how to use those with this x68i5 board ?
Oh great, thank you @Seeed_huang !
And is there an explanation anywhere how to use these in software ? (i.e. access them via c/c++ code)
Maybe something like Accessing 40-pin GPIO | Seeed Studio Wiki but for X86i5 board and these pins ?
My goal is still to be able to connect an IMU to the X86i5 board for real-time interaction through c/c++. I saw that there is a guide for Arduino here but I’m not sure this can be applied to X86i5 board.