I see this in the two data sheets, Looks like FIFO and Android compatibility Diff.
LSM6DS3
Smart FIFO up to 4 kbyte based on features set
Android M compliant
LSM6DS3TR-C
Smart FIFO up to 8 kbyte based on features set
Compliant with Android K and L
It’s been discussed b4 HERE
I believe the library address the same functions.
我们制作的这个库的功能应该是可以应用在XIAO BLE上的,如有不能使用的功能,可以向我们提供相关反馈,谢谢。
LOL
or “The functions of the library we made should be applicable to XIAO BLE. If there are functions that cannot be used, please provide us with relevant feedback, thank you.”
Seed technical didn’t dispute so ?
HTH
GL ![]()