I have collected another image as much as possible for ReSpeaker Core v2. All details are in the description. Be sure to make a re-layout for the SD card to expand the root system.
You can get acquainted with the new wikipedia for ReSpeaker Core v2. where I personally went through all the ways and fully tested it. All I have written is a working solution for 2023
Image respeaker-debian-11-sd-8gb-xrdp-mdp-rhasspy-hlc-noise-11042023.img.gz
Описание
- Debian 11 with all updates
- SFTP access is enabled - root access - Read the details here
- SSH access is enabled - you can immediately connect to ReSpeaker via the Putty console
- Custom SSH banner - Read the details here
- LEDs are working
- Sound works - Read the details here
- The microphone works
- The button works
- Installed Rhasspy 2.5.11 - Read the details here
- HermesLedControl is installed - Read the details here
- The inclusion of LEDs is included in the startup - Read the details here
- XRDP is installed - Read the details here
- MPD is installed - Read the details here
- Noise reduction is enabled (Choose Microphone Noise microphone) - Read the details here
Accounts
User respeaker
Login: respeaker
Password: 12345678
User root
Login: root
Password: 12345678
Installation
- Install to SD card via balenaEtcher program