If you are fighting with noise from the buck converter (XIAO RA4M1), there is a solution

Hi friends, the buck converter (SGM6029) can cause problems with sensitive peripherals: I could not filter out the noise on VBat to run a DCF77 receiver module. Sometimes there are also reports of problems with the ADC with very small signals.

I was able to save my project by removing the buck converter (just push it away with a pin) and installing a diode (e.g. 1N4148 SMD) as shown. This is not difficult and takes 10 minutes. Instead of 3.3V you now have 3.2V~3.5V (depending on the charge state) and ~4.5V during the charge state! You can enable the internal reference (1.45V) for the ADC.

I also took the opportunity to change the charging current for the charging unit, as 150mA is too high for small batteries. There for I changed R10 (yellow arrow): Original ICharge=24000/160K = 150mA, now ICharge=24000/482K = 50mA.

Unfortunately this is difficult (SMD 0201)

Hi there,

Wow, Welcome to the 3rd LEVEL :grin: :point_up:
Excellent deduction, and Solution finding as well. Seeed Engineering may have to take a look and see if this is a systemic issue or just a wonky Batch?
I appreciate the extra effort and fine quality post. How did you solder?, “Hot Tweezers” or air? Very, cool indeed.

GL :slight_smile: PJ :v:

thanks for the kind words! It is sometimes easier to mechanically destroy components at both ends with a needle beforehand and then desolder the ends separately. I solder them under a microscope with a very fine soldering tip. I have experience with several hundred LEDs :innocent:

LED_Watch Achieves a Quasi-Analog Display with 240 LEDs and Unique Etching Technique - Hackster.io

Wow your projects are super cooooooool!

Hi there,

Jesus man …thay have a name for people like you…“perfectionist”
WOW,

I had to share this one… The BEST or even better picture is on the LINK… Everyone should hit your link and see this project … WOW
Thanks for the effort…WOW! :star_struck:

GL :slight_smile: PJ :v: