Seeeduino V4.2 , if push reset button , could erase firmware or not?
Hi there,No, If you press the reset button, it only restarts the board, similar to unplugging and plugging back the energy. thanks.
Hi ,
If I want re-upgrade firmware of seeeduino V4.2 , where can to download firmware.
Thanks.
Hi there,
Please download the file and it includes the instructions and firmware. 
<LINK_TEXT text=“https://github.com/SeeedDocument/forum_ … o_boot.zip”>https://github.com/SeeedDocument/forum_doc/raw/master/reg/seeeduino_boot.zip</LINK_TEXT> Thanks
Hi there,
I need re-upgrade which one of MCU boot or interface boot ?
Thanks.
Hi  there,
The Interface one is near the USB and the MCU one is near SPI. 
Thanks