(IDEA) Can Rephone Breakout Be linked to WS2812 led?

Hi,

Wondering if WS2812 x12 (neo pixel ring) can be connected to Xadow Breakout?
Without xadow duino connected to rephone mainboard.

Any ideas?

Thanks!

Just use external power for the neopixel ring, connect the 2 ground points and choose 1 digital output pin on the breakout board. It’s that easy!

What’s a ws2812b library that will work on the Rephone? The neopixel library is not compatible.

Thanks.

Yeah how do we program the ws2812 through the breakout board? Thanks!
is there a sample code and connection layout available?