Hi,
I have one of your 0.5 Inch OLED display Arduino shields.
Unfortunately I do not get it to work in I2C mode (resistors changed accordingly…) together with the U8G2 lib on my Arduino Micro and Arduino MicroPro. (I used HW pins 2 and 3 for I2C connection)
SPI Mode works perfectly with the display and u8g2 lib…
Can you please advice or provide a sample code and wirering schematic please to use the u8g2 lib.
Thank you
Best regrads
Eike
My code look slike this:
note: none of the constructors works for I2C…
#include <U8g2lib.h>
//U8G2_LD7032_60X32_F_4W_SW_SPI u8g2(/rotation/U8G2_R0, /* clock=/ 3, / data=/ 2, / cs=/ 7, / dc(A0)=/ 6, / reset=/ 8);
//U8G2_LD7032_60X32_F_2ND_4W_HW_SPI u8g2(/rotation/U8G2_R0,/ cs=/ 7,/ dc=/ 6,/ reset=/ 8);
//U8G2_LD7032_60X32_F_SW_I2C u8g2(/rotation/U8G2_R0,/ clock=/ 3,/ data=/ 2); //, /reset=/ 8)
//U8G2_LD7032_60X32_F_HW_I2C u8g2(/rotation/U8G2_R0);
U8G2_LD7032_60X32_F_HW_I2C u8g2(/rotation/U8G2_R0, /reset=/ 8);//,/ clock=/ 3,/ data=*/ 2);
void setup(void) {
u8g2.begin();
}
void loop(void) {
u8g2.clearBuffer(); //lösche bildschirm puffer
u8g2.sendBuffer();
u8g2.setFont(u8g2_font_profont10_tf);
u8g2.drawStr(0,20,“Hello World!”);
u8g2.sendBuffer();
delay(200);
}
Basically it should work. Can you post a picture of your setup?
Oliver
Same question here: https://github.com/olikraus/u8g2/issues/865