I2C Module Problems with Grove Beginner Kit for Arduino

Yes, software I2C works, even with the pullup resistor problem.
This is an OK workaround, but isn’t a fix for the hardware bug.
And, software I2C is slower, which could be a problem for some projects.

I’d rather use hardware I2C.
Will Seeed Studio be redesigning the Grove Beginner Kit to resolve this problem?
And, will existing customers get replacement boards?
Or, perhaps, some sort of Grove connector with pullup resistors?
(I’m using 3.9K pullups on the SDA and SCL lines when only the OLED is connected to the I2C bus.)
And will customers that have old boards get corrected 3-Axis Acceleration Modules?

Also, will Seeed Studio update the Lesson Guide to explain the issue, workarounds, and replacement process?

Without a complete resolution of the problem, I will not be able to continue to use the Grove Beginner Kit for my university and K-12 classes. I will mostly likely use the Sparkfun RedBoard with QWIIC modules instead.