I want to solder the terminal resistor on the recomputer R1000 board so the RS485 can function perfectly. I don't know where to solder the 120ohm terminal resistor.

Hello,
You need to go and solder the 120Ω resistor in the position shown in the picture.

good job buddy! you made it over here i think you are trying to communicate way too fast

do you know why they would leave this resistor out? i am not seeing the reason

Hi there,
it’s based on the resistance, type of signalling, P2P or MultiPoint, or MultiDrop.
2-wire half duplex or 4Wire FDX. RS-485 is the most versatile interface of them all.
It was the first balanced driver , long run interface from back in the day. Supports a Master/Slave or Multiple slaves in a multiDrop configuration.

HTH
GL :slight_smile: PJ
:v:

It’s not unusual to have extra resistors along for changing the levels or match longer runs, or multi drop.
RS-232C and RS-485, or even RS-422 weret he standards back in the Day. :+1:

In simple terms, when communicating via RS485, there needs to be a pull-up resistor, and this pull-up resistor should be either on the sensor end or the device end. To allow sensors with built-in pull-up resistors to work normally on the R1000, we have defaulted to not including the pull-up resistor, but have provided solder pads for users to add one if needed.

thanks very good answer!