Hii ,
I connect ESP WROVER32 connect with Seeed sensor ,so i used this github:-GitHub - limengdu/Seeed-Studio-MR24FDB1-Sensor: Seeed_24GHz_mmWave_Radar_Sensor
but I could not getting data of sensor using this code , Please suggest me any documentation and code
I will connect the arduino with uart pin TX and RX
You can follow this wiki:
but the mcu used in wiki is xiao esp32c3, not ESP WROVER32
Any other ESP board is working expect XAIO ESP32C3
Hi there,
Of course you can make it work if you use the correct pins…
HtH
GL
PJ
@PJ_Glasso Hii
Actually we should interfacing the pin of GPIO 16 RX or 17 TX pin but the esp32 Wroom 32 e is reset self
Please give any suggestion or documentation
I found this error while geeting the data with esp32wroom
rst:0x8 (TG1WDT_SYS_RESET),boot:0x13 (SPI_FAST_FLASH_BOOT)
configsip: 0, SPIWP:0xee
clk_drv:0x00,q_drv:0x00,d_drv:0x00,cs0_drv:0x00,hd_drv:0x00,wp_drv:0x00
mode:DIO, clock div:1
load:0x3fff0030,len:1344
load:0x40078000,len:13964
load:0x40080400,len:3600
entry 0x400805f0
ets Jul 29 2019 12:21:46
Hi there,
Yes the Output is indicating, a WatchDogTimer caused System Reset. probably because the SPI is jammed and didn’t respond.
Post the code, use the code tags we can look and make suggestions.
HTH
GL
PJ
@PJ_Glasso I used this library -GitHub - limengdu/Seeed-Studio-MR24FDB1-Sensor: Seeed_24GHz_mmWave_Radar_Sensor
and connect with sensor and this code I am using
#include <falldetectionradar.h>
FallDetectionRadar radar;
void setup()
{
radar.SerialInit();
Serial.begin(9600);
delay(1500);
Serial.println(“Readly”);
}
void loop()
{
radar.recvRadarBytes(); //Receive radar data and start processing
if (radar.newData == true) { //The data is received and transferred to the new list dataMsg[]
byte dataMsg[radar.dataLen+1] = {0x00};
dataMsg[0] = 0x55; //Add the header frame as the first element of the array
for (byte n = 0; n < radar.dataLen; n++)dataMsg[n+1] = radar.Msg[n]; //Frame-by-frame transfer
radar.newData = false; //A complete set of data frames is saved
//radar.ShowData(dataMsg); //Serial port prints a set of received data frames
radar.Situation_judgment(dataMsg); //Use radar built-in algorithm to output human motion status
}
}