I need help with the SenseCAP Card Track T1000-E

Ah, now I understand. Sorry, I’m not familiar with Fahrenheit temperature values, and I didn’t recognize the already provided answer. OK, then the tracker provides temperature measurements. Thanks for clearing that up. Can an other node also access the temperature measurements of that 5f5a tracker?

interesting question… i dont have two T1000-E… but I do have a T1100… I will try to do some experiments

Pin List​

Power to Sensor P0.4 GPIO
Temperature P0.31 NTC (analog)
Light P0.29 LUX(analog)
3-Axis Accelerometer
(Not currently used in the Meshtastic firmware) SDA: P0.26
SCL: P0.27 Via IIC
Power to Accelerometer P1.7 GPIO
LED P0.24 GPIO
Buzzer P0.25 GPIO
Enable Buzzer P1.05 GPIO
Button P0.6 GPIO
Power to sensor P1.6 GPIO
LR1110 P1.08: SPI MISO
P1.09: SPI MOSI
P0.11: SPI Clock
P0.12: SPI NSS
P1.10: LoRa Reset
P1.01: LoRa DIO1
P0.07: LoRa DIO2
LR11X0_DIO3_TCXO_VOLT
AGE 1.6V SPI
GPS RX: P0.14
TX: P0.13 Serial1
BAUDRATE:115200

The F temp system is used primarily in the USA, which is opposed to the metric system.

The F system is basicly used to discribe temp range that a human person is likely to encounter in the environment. 0 being slightly colder than freezing and 100 being slightly colder than hot as hell

the C temp system, in contrast is 0 at the freezing point of water at normal temp and pressure and 100 being the boiling temp of water at normal temp and pressure

it is easier to hear an american say its hot as hell in here… and someone say how hot is it… and they say 100 F-ing degrees F as opposed to 38 deg C…

we are so melodramatic…

I like if manufacturers deliver PIN Lists. In the teardown video I saw, that that case is really not made to be opend. So having a PIN List is cool, but there seems to be no way to access those PINs without destroying the trackers case.

You access them thru the software


Example of position inaccurate of a stationary unit

Example of fake weather data skimmed from the internet based on location… I do not like when they do this… I don’t need a tracker to make up fake data for me to know about

1 Like

This toggle weather under device app settings will change from fake weather to actual sensor data… what da?

This GPS position flickering is artificially caused. To prevent military use of public available GPS data it is altered automatically before transmitting.