I have a Grove Base Shield and it seems that it does not work with Arduino Mega and it works for Arduino Uno (it says it is compatible to Arduino Mega)

Hi Bill,

Thanks a lot for your quick response! I connected the base shield v2 to Arduino mega. Then I connected a Grove GPS v1.2 (Sim28) to the base shield using D2. There is no GPS reading. If I use Arduino Uno, then there is GPS reading. That is why I said that it seems this base shield is not compatible with Arduino mega. Is there something I am missing?
Best regards,

Jian