I am looking for an Amazon-Echo-like device to capture voice for a speech recognition system I am working on

Hi there,
I am looking for an Amazon-Echo-like device to capture voice for a speech recognition system I am working on.
I would like to have the following feautures:

  • (Mandatory) the device can be set up so that it takes the predominant voice. So if there are other distant voices, it should remove them.
  • (Mandatory) the device will remove noises, echos,… that is, do some voice enhacenment.
  • (Mandatory) PC must recognize it as an input audio device.
  • (Optional) the device can be set up so that different voices captured from different microphones can be separated in different audio channel.
    Is any of your ReSpeaker good for that?
    Also, I live in Spain. Do you ship there?
    Thanks

Hi there,


You can consider ReSpeaker Mic Array v2.0. Here is the detail info.