Hi,
thanks for your quick response!
I am already starting the server manually. This is the output:
-
When creating new wio link node:
[I 160430 12:35:23 handlers:86] get current user, id: 26, email: <>
[I 160430 12:35:23 web:1946] 200 POST /v1/nodes/create?name=node000&board=Wio+Link+v1.0 (127.0.0.1) 20.31ms -
After entering wifi key, wio name and submitting (with android app)
[I 160430 12:36:01 handlers:86] get current user, id: 26, email: <>
[I 160430 12:36:01 web:1946] 200 GET /v1/nodes/list (127.0.0.1) 6.26ms
(multiple times, then timeout)
So the app is polling for changes on the server.
Problem is, that the Wio itself does not connect to the server, although wifi connection is established (confirmed via fritzbox log)
The led is blinking twice first, while connecting to wifi. The it starts blinking shortly once while trying to connect to server and stays is this state, even after the timeout.
Any other idea? 
Most importantly ther is no access to the apache server from the Wio itself, only from the android phone, I use.
[I 160430 12:33:39 server:535] SQLite version: 3.8.7.1
[I 160430 12:35:23 handlers:86] get current user, id: 26, email: <<censored>>
[I 160430 12:35:23 web:1946] 200 POST /v1/nodes/create?name=node000&board=Wio+Link+v1.0 (127.0.0.1) 20.31ms
[I 160430 12:36:01 handlers:86] get current user, id: 26, email: <<censored>>
[I 160430 12:36:01 web:1946] 200 GET /v1/nodes/list (127.0.0.1) 6.26ms
...and so on