[HowTo] [updated] Install the WIO Server on Raspberry Pi 3

Hello Kai,
do you see a different behaviour of the blue LED if you connect to the international server and your own server? It should blink every second.

Try the following:
stop the automatic start of the server by editing the file “/etc/rc.local” again. Delete the inserted line or comment out by putting a hash (#) in front of the line.

Restart the PI and enter

cd /opt/Wio_Link python server.py

Ther server should start now and you should see the communication, for example

[I 160430 10:13:30 server:535] SQLite version: 3.8.7.1 [I 160430 10:13:32 server:432] xchange device server accepted conns: 1 [I 160430 10:13:32 server:136] accepted sn: {your serial number here} @fw_version 1.1 [I 160430 10:13:32 server:165] valid hello packet from node 104 [I 160430 10:13:32 server:429] ota device server accepted conns: 1 [I 160430 10:13:32 server:136] accepted sn: {your serial number here} @fw_version 1.1 [I 160430 10:13:32 server:165] valid hello packet from node 104 [I 160430 10:14:32 server:306] heartbeat sent to node 104 on xchange channel [I 160430 10:14:32 server:306] heartbeat sent to node 104 on ota channel [I 160430 10:14:32 server:224] Node 104 alive on xchange channel! [I 160430 10:14:32 server:228] Node 104 recv json on ota channel

Or do you see any error messages?