[HowTo] [updated] Install the WIO Server on Raspberry Pi 3

Hello uwe.fetzer, under Configure SSL when you say "Make sure, that you enter your (local) domain name at “Common name (FQDN), for example “*.se38.local” " where do you get your (local) domain name? Do you need a real FQDN? My server on a BBB is just local and only has an IP address with a local name. Everything I did will be at home and behind a firewall so I dont understand this step. Also you do not mention Steps 2.4 to 2.6.

I have a problem with 2.4 The command “supervisor” is to run the server at startup with the config file esp8266_server.conf. This file refers to " directory=/root/esp8266_iot_node/"
& “command=python /root/esp8266_iot_node/server.py”. In the whole process up to this stage this directory was never created. Using ubuntu command find / -name “esp8266*” -type d, the only files containing “esp8266*”. These are:
/opt/xtensa-lx106-elf/bin/Wio_Link/esp8266_arduino
/opt/xtensa-lx106-elf/bin/Wio_Link/esp8266_sdk
/usr/local/bin/Wio_Link/esp8266_arduino
/usr/local/bin/Wio_Link/esp8266_sdk

There is no directory at /root/esp8266_iot_node/. What is the correct directory? The command
“sudo supervisorctl start esp8266” fails.

Did you include the step, “2.6 Block 8080 port”? I can not get the command “supervisorctl restart esp8266” to work.
Thanks
Philip