How to upgrade to Jetpack 6.1 without Ubuntu. Need to download Jetpack 6.1 Manually

Can someone help me to figure out how to manually download Jetpack 6.1 to install on directly on my installed NVME on my Jetson Orin Nano. I run Fedora on my desktop not ubuntu, so I cannot utilize the Nvidia SDK Manager to pull down SDKs. On fedora I see “No available releases for host OS: Fedora 41”

Should I just use the sd card image?

Hi there,

and Welcome here…

So have you seen this thread ? " How to Upgrade from Jetpack 6.0 to Jetpack 6.1 using SD card method and Debian package upgrade?"

HTH
GL :slight_smile: PJ :v:

Thanks for the reply, however that is on Ubuntu which will fetch the jetpack automatically for you.

Interestingly enough, you can install the Nvidia SDK manager on Fedora via rpm, however Nvidia apparently does not support the upgrade/flash on Fedora