Thanks! Not knowing better, I have in fact been using lib 2.22 together with app 2.50 and that also worked. Now I have tried to update to lib 2.5 and the update process seems to work. However, the splash screen still says “2.22”…
If you use the same version 2.2 files for the lib, there should not be any reason to rebuild the dfu and call it 2.5, or am I missing something? I would just have shipped an DSO201_LIB_V2.2.dfu together with the DSOnanoAPP2.5.dfu, to avoid any confusion…
I installed the lib first and then the app - used the process in the manual for the most part - used DfuSE Demo 3.0.1 with Win7 x64. Also the program barked a warning that the device was in dfu mode so it could not verify etc, I clicked ok (but only after I downloaded the existing dfu form the DSO first to have a backup). One feature I was hoping for was to loose the waveform at startup, not big deal though - really liking this thing.