How to flash firmware to an RHF76-052

Hello,

Recently I had trouble writing to an RHF76-052 and I did something wrong I guess, because after a few attempts and reconnecting it is not getting recognized by any pc anymore, not Linux neither Windows. So I guess Arduino overwritten something it should have not overwritten, or the device did some kind of firmware update which failed.

The thing that caused is does not matter, I’m wondering how I can flash something onto the RHF76-052. Currently I need to flash rhf76-052am-v2.0.10-20160923.ebin 2.bin to it, with the hope that it will work.

Already thanks for helping, and have a great day !