I have a Jetson Xavier NX and an IMX219-83 8MP 3D Stereo Camera Module. I have connected the camera to the Jetson with the provided FFC cable. I have a few questions though:
- What do the lights on the camera mean? It is showing a single red LED, is that good or bad?
- Do I need to connect it with the provided PH2.0 4 pin wire as well?
- How do I actually connect to the camera on my Jetson and see the two camera outputs?