I have a version 1.0 Rainbowduino (no USB power, FTDI connection) and I recently also got a Rainbowduino 3.0.
There is a very nice Rainblow_Plasma sketch that I have running on the Rainbowduino 1.0, but I can’t seem to get it to run on the Rainbowduino 3.0.
It compiles OK but just has a single flickering line of LEDs. The Rainbowduino 3.0 examples compile and run perfectly.
Is there any documentation on what changed between Rainbowduino 1.0 and Rainbowduino 3.0? Is the hardware more or less compatible, or did it change a lot? Also, can the Rainbowduino 3.0 library be used to code for the older Rainbowduino?