How to compile a USB wifi driver?

Hi all,

I have a problem. My respeaker can’t found some SSIDs on the CISCO wi-fi access point.

So, I have tried to connect via USB wi-fi card to the access point,

and I have compiled the USB wi-fi driver, but I can’t.



I don’t know exactly but I know that to compile a driver, I need ‘/scripts/recordmcount’

To compile ‘/scripts/recordmcount’, I execute ‘make scripts’ like the followings.



----------------------------------------------------

respeaker@v2:/usr/src/linux-headers-4.4.138-respeaker-r0$ sudo make scripts

scripts/kconfig/conf --silentoldconfig Kconfig

*

  • Restart config…

    *

    *
  • General setup

    *

    Cross-compiler tool prefix (CROSS_COMPILE) []

    Compile also drivers which will not load (COMPILE_TEST) [N/y/?] n

    Local version - append to kernel release (LOCALVERSION) []

    Automatically append version information to the version string (LOCALVERSION_AUTO) [N/y/?] n

    Default hostname (DEFAULT_HOSTNAME) [localhost] localhost

    Support for paging of anonymous memory (swap) (SWAP) [Y/n/?] y

    System V IPC (SYSVIPC) [Y/n/?] y

    POSIX Message Queues (POSIX_MQUEUE) [Y/n/?] y

    Enable process_vm_readv/writev syscalls (CROSS_MEMORY_ATTACH) [Y/n/?] y

    open by fhandle syscalls (FHANDLE) [Y/n/?] y

    uselib syscall (USELIB) [Y/n/?] y

    Auditing support (AUDIT) [N/y/?] n

    Kernel .config support (IKCONFIG) [Y/n/m/?] y

    Enable access to .config through /proc/config.gz (IKCONFIG_PROC) [Y/n/?] y

    Kernel log buffer size (16 => 64KB, 17 => 128KB) (LOG_BUF_SHIFT) [18] 18

    CPU kernel log buffer size contribution (13 => 8 KB, 17 => 128KB) (LOG_CPU_MAX_BUF_SHIFT) [12] 12

    Checkpoint/restore support (CHECKPOINT_RESTORE) [N/y/?] n



    …



    CC scripts/mod/empty.o

    gcc: error: unrecognized command line option ‘-mgeneral-regs-only’

    scripts/Makefile.build:277: recipe for target ‘scripts/mod/empty.o’ failed

    make[2]: *** [scripts/mod/empty.o] Error 1

    ----------------------------------------------------



    Does anyone know solve this error?

    gcc: error: unrecognized command line option ‘-mgeneral-regs-only’

Hi n-shinkai,



Are you using the 2.4Ghz network or 5Ghz? and it only supports 2.4Ghz network.