I had made a project using seeed xiao esp32c3. I had connect the battery to it using the backside pins now i wanted to hiw to charge the battery again please help me.
charge by connecting to usb
is this the only other way, with out using an external BMS?
I thought I’d be able to connect directly to the board, a USB 5v input, 1A to 3A’s, using the VBUS and GND.
Hi there,
“Yes” The battery will be recharged by the onboard charge controller, if the USB-C is connected.
I would look to the schematic and see if connecting the 5V source directly to Pin VCC(5V) of Xiao
will work as long as NO other usb device is plugged in.
HTH
GL
PJ ![]()