OK, this is a pretty neat electronic toy, but I am getting bugged by the waveform in the background which is there on every boot. How can I get rid of it? I have been able to load and save my own waveforms, but that “default” one will just not go away, even when I load my own saved ones. I noticed that the screen refreshes do seem to tear up the image of the default waveform, but it just ends up cluttering everything up.
There are also artifacts displayed from moving waveforms that stick around which also clutter things up. Sorry if it sounds like I am bagging on the v2, I really like it and can overcome these problems, though I would rather not have to. I have the V2 with App ver2.40. Thanks!
By the way, I found that a SanDisk 2GB microSD Card (Buy.com sku 209632621) worked after I formatted it with “FAT” from windows 7. Another answer to a question probably only I would have is that the SD goes in with pins up (I found it a bit fiddly and did not want to force anything, and then it just went in - hehe).