How about ESP32+CAN FD+LoRa?

:alarm_clock:New Product idea! This week, Seeed studio released the first prototype of a small developer board based on the community’s voice, which combines ESP32+CAN FD+LoRa.

:eye_in_speech_bubble: Feel free to let us know if you like it and tell us what you want us to add!

:point_right:For more information:Voice Needed! Do you know XIAO ESP32C3 can CAN? - Latest Open Tech From Seeed (seeedstudio.com)

Does it support Arduino IDE?

YES! Late I will update the key feature list of this board.

Hi community, here is the key features of ESP32+CAN FD+LoRa

  • ESP32 micro-controller supported
  • CAN FD supported
  • WiFi, Bluetooth and LoRa supported
  • Up to 10km long-distance RF performance
  • Wide range 4.5V-28V power supply input
  • Arduino IDE supported

Thanks a lot. sounds like a good product.

1 Like