Hi,
I watched this video for HM-10 that shows pairing master/slave with two BLE modules:
I have two problems:
-
HM-11 BLE BEE in Uartsbee (V4 and V5) does not respond to any AT commands (AT should return OK at 9600baud rate). Uartsbee is connected to PC and I have console open. When switching from HM-11 to Meshbee, setting 115200baud and issuing +++ returns answer to the console. So the problem is that BLE BEE is not responding. PWR led on Uartsbee is steadily on. LED with name ‘ON’ is blinking on Uartsbee.
-
I have two XADOW BLE modules with two mainboards. In slave mode they work ok. I can receive and send data to Android tablet with BLE. Now I turn off BLE on Android and want to connect two Xadow BLE to each other. AT+ROLE0 returns OK+SET0. AT+ROLE1 on other device returns OK+SET1. According to the Youtube video, it should now return also OK+CONN. But this never happens.
I bought it like 6 months ago and still cannot solve this
…tried also other AT commands from data sheet such as AT+DISC? for discovery. But your demo source code does not work for me: seeedstudio.com/wiki/Xadow_-_BLE …only AT+ROLE[] command works, but it’s not pairing with the master.
Please help, I’m lost 
Your antispam didn’t like offsite links. So here the Youtube video: youtube com/watch?v=nliVeSmpFgg
Right now I’m going to test Bees shield+Seeeduino V3 with BLE Bee. There is some RX/TX jumper for console debug…glad I bought more solutions 
Got it tha pairing working. Had to use Bee Shield+Seeeduino V3. AT commands works only with delay?
#define SerialBaud 9600
#define Serial1Baud 9600
void setup()
{
Serial.begin(SerialBaud);
Serial1.begin(Serial1Baud);
while(!Serial.available());
// set master
Serial1.print("AT+CLEAR");
delay(1000);
Serial1.print("AT+ROLE1");
delay(1000);
Serial1.print("AT+DISC?");
delay(1000);
}
void loop()
{
//Serial1.print("test I am slave ");
//delay(10000);
if (Serial.available())
{
Serial1.write(Serial.read());
}
if (Serial1.available())
{
Serial.write(Serial1.read());
}
}
This will return: OK+CLEAROK+SET1. But AT+DISC? should return something as well. On the other side I did run: AT+ROLE0 and now it has paired!!
Seeeduino V3 with SoftSerial:
#include <SoftwareSerial.h>
SoftwareSerial mySerial(7, 8);
void setup() {
Serial.begin(9600);
Serial.println("Goodnight moon!");
// set the data rate for the SoftwareSerial port
mySerial.begin(9600);
mySerial.println("Hello, world?");
delay(1000);
}
void loop() {
// run over and over
if (mySerial.available()) {
Serial.write(mySerial.read());
}
if (Serial.available())
mySerial.write(Serial.read());
}
However I can send only from master to slave. Slave to master does not print anything. Also characters from master to slave are muffled - looks like a wrong baud rate or something. But I tried issuing AT+BAUD0 on both and am setting 9600 serial speed on both as well. Arduino Console is set to 9600 too.
UPDATE: Right now I plugged the BLE back to Uartsbee V5 (UART mode) and Xadow BLE can talk to each other! But characters are still muffled.
It prints
ÿ
for each character no matter if I type a, b, 1, 0…
I’m using Windows 7 by the way.
So the HM-11 in Uartsbee had a different baud rate. Now it works both sides! 
Still don’t know how can I issue AT commands through Uartsbee…