Hi all!
I’ve just got myself an ESP32C3 board and wanted to tinker with it to achieve the following (ambitious?) goal:
- On ESP power-on/boot, have two wires shorted/connected by default to replicate a DIP-SWITCH in the ON position.
- If at ESP power-on/boot and before a period of 5 seconds, the board detects that a (tiny) Push-Button is in the OFF position (open/no short), then it will disconnect/open the two shorted wires (DIP-ON) so it is OFF (DIP-OFF). After those 5 seconds have passed, it will not react to any changes of this push-button trigger untill you power-cycle the ESP.
I don’t want to inject any kind of power (like the led example) into the two cables that need to be controlled (open/closed on/off).
Is that possible?
If so, how would I go about it code wise with Arduino IDE and what pins would I use? ADC?
My head is spinning so any help or pointers would be inmensly appreciated!
Thank you! ![]()