/*
BluetoothBee Demo Code - Flowcontrol Based Implementation
2010,2011 Copyright (c) Seeed Technology Inc. All right reserved.
Author: Visweswara R
This demo code is free software; you can redistribute it and/or
modify it under the terms of the GNU Lesser General Public
License as published by the Free Software Foundation; either
version 2.1 of the License, or (at your option) any later version.
This library is distributed in the hope that it will be useful,
but WITHOUT ANY WARRANTY; without even the implied warranty of
MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
Lesser General Public License for more details.
You should have received a copy of the GNU Lesser General Public
License along with this library; if not, write to the Free Software
Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA
For more details about the product please check seeedstudio.com/depot/
*/
/* Upload this sketch to Seeeduino and press reset*/
#include <NewSoftSerial.h> //Software Serial Port
#define RxD 0
#define TxD 1
#define DEBUG_ENABLED 1
NewSoftSerial blueToothSerial(RxD,TxD);
void setup()
{
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
}
void loop()
{
//Typical Bluetoth command - response simulation:
//Type ‘a’ from PC Bluetooth Serial Terminal
//See Bluetooth Bee - Wiki for instructions
if(blueToothSerial.read() == ‘a’)
{
blueToothSerial.println(“You are connected”);
//You can write you BT communication logic here
}
}
void setupBlueToothConnection()
{
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
delay(1000);
sendBlueToothCommand(“\r\n+STWMOD=0\r\n”);
sendBlueToothCommand(“\r\n+STNA=SeeeduinoBluetooth\r\n”);
sendBlueToothCommand(“\r\n+STAUTO=0\r\n”);
sendBlueToothCommand(“\r\n+STOAUT=1\r\n”);
sendBlueToothCommand(“\r\n +STPIN=0000\r\n”);
delay(2000); // This delay is required.
sendBlueToothCommand(“\r\n+INQ=1\r\n”);
delay(2000); // This delay is required.
}
//Checks if the response “OK” is received
void CheckOK()
{
char a,b;
while(1)
{
if(blueToothSerial.available())
{
a = blueToothSerial.read();
if('O' == a)
{
// Wait for next character K. available() is required in some cases, as K is not immediately available.
while(blueToothSerial.available())
{
b = blueToothSerial.read();
break;
}
if('K' == b)
{
break;
}
}
}
}
while( (a = blueToothSerial.read()) != -1)
{
//Wait until all other response chars are received
}
}
void sendBlueToothCommand(char command)
{
blueToothSerial.print(command);
CheckOK();
}