n3em3o
1
Hello, I just bought a passive buzzer, and I want to use it on raspberry pi.
But look at wiki saying it can only be used on add. What can I do now?
n3em3o
2
Also, I run the LED button program, the error is as follows
Baozhu
4
Sorry, the wiki hasn’t been updated in time.I’ve got a document for you to refer to.
n3em3o
5
Also, I run the LED button program, the error is as follows
Baozhu
6
LED Button Program is just GPIO programming. https://pypi.org/project/RPi.GPIO/
n3em3o
7
Can I check if I press the button???
Baozhu
8
Of course, This library is also suitable for input devices.