help me plz cant convert to string value

hi im rookie

i buy Grove-Laser_PM2.5_Sensor-HM3301 im try edit code new format for keep in var and return value. but it error cant convert to string







//start hm3301



HM330X sensor;

uint8_t buf[30];



const char *str[] = {"sensor num: ", "PM1.0 concentration(CF=1,Standard particulate matter,unit:ug/m3): ",

"PM2.5 concentration(CF=1,Standard particulate matter,unit:ug/m3): ",

"PM10 concentration(CF=1,Standard particulate matter,unit:ug/m3): ",

"PM1.0 concentration(Atmospheric environment,unit:ug/m3): “,

“PM2.5 concentration(Atmospheric environment,unit:ug/m3): “,

“PM10 concentration(Atmospheric environment,unit:ug/m3): “,

};



HM330XErrorCode print_result(const char *str, uint16_t value) {

char newformat;

if (NULL == str) {

return ERROR_PARAM;

}

//SERIAL_OUTPUT.print(str);

//SERIAL_OUTPUT.println(value);

newformat = str + “=” + value;

return newformat;

//return NO_ERROR;

}



//parse buf with 29 uint8_t-data

HM330XErrorCode parse_result(uint8_t *data) {

uint16_t value = 0;

char resultpm;

if (NULL == data)

return ERROR_PARAM;

for (int i = 1; i < 8; i++) {

value = (uint16_t) data[i * 2] << 8 | data[i * 2 + 1];

//print_result(str[i - 1], value);

resultpm += print_result(str[i - 1], value);

if(i < 7){

resultpm += “, “;

}

}

return resultpm;

//return NO_ERROR;

}



HM330XErrorCode parse_result_value(uint8_t *data) {

if (NULL == data) {

return ERROR_PARAM;

}

for (int i = 0; i < 28; i++) {

//SERIAL_OUTPUT.print(data[i], HEX);

//SERIAL_OUTPUT.print(” “);

if ((0 == (i) % 5) || (0 == i)) {

//SERIAL_OUTPUT.println(””);

}

}

uint8_t sum = 0;

for (int i = 0; i < 28; i++) {

sum += data[i];

}

if (sum != data[28]) {

SERIAL_OUTPUT.println(“wrong checkSum!!!”);

}

//SERIAL_OUTPUT.println(””);

return NO_ERROR;

}



//end hm3301





void loop() {



//hm3301

//parse_result_value(buf);

//parse_result(buf);

//SERIAL_OUTPUT.println(””);





String postData = sensorName + “,sensorType=BME680 temperature=” + t + “,pressure=” + p + “,humidity=” + h + “,gas=” + g;

int httpCode = http.POST(postData);

SERIAL_OUTPUT.print(httpCode);

SERIAL_OUTPUT.print(” : ");

SERIAL_OUTPUT.println(postData);



String postData2 = sensorName + “,sensorType=HM3301 " + parse_result(buf); <<< i want to send this format style

int httpCode2 = http.POST(postData2);

SERIAL_OUTPUT.print(httpCode2);

SERIAL_OUTPUT.print(” : ");

SERIAL_OUTPUT.println(postData2);



}







Anyone help me please. ty so much Anyone.

Hi,



Did you checked Arduino JSON