Hi there,
I am having some problems trying to use the grove - I2C motor driver. I installed the library I found on this wensite, grove_I2C_motor_driver. Unfortunately I can not find or open the examples that should have been included in the library. However if I go to Arduino IDE -> manage libraries, the library seems to be installed. And the examples are in the folder but they are not accessable through the examples in the IDE but the files of the examples are the zip folder. Did someone else encounter this problem?