i wanted to run the GrovePi+ (on a RPi 3B+) with the “Grove - I2C Motor Driver (TB6612FNG)” (of course to run a motor with it).
But i think I got the wrong combination?
Would I need the Base Shield?
Or is there a way to run the GrovePi+ with the Motor Driver?
I struggle a little bit cause i dont know where to start.
Edit:
I tried it anyway, but I got the following Error:
After running the following command:
“sudo python3 -m pip install raspberry-i2c-tb6612fng”
Error:
“Could not find a version that satisfies the requirement raspberry-i2c-tb6612fng (from versions: )
No matching distribution found for raspberry-i2c-tb6612fng”
I think its because i try to run it on “Linux dex 4.19.66-v7+” / “Raspbian For Robots” ?
I think you don´t mean a problem that the Pi can`t connect to the internet in generally? I can connect to the Pi via SSH and also via VPN. I also can ping from the Pi for example to “8.8.8.8” without any problem.
Do you mean that there is maybe a problem to connect to the server where I should can download the package?
I have checked some things I found online, for example:
pi@dex:~ $ curl https://pypi.org --> my IP isnt Blacklistet (but this was not the exact link to the package i think?)
I want to try to download it via “wget” but I dont know the exact adress I would have to enter
What could I do next to solve or at first localize the error?
My first thought was, as i wrote, that it is some problem with the OS im running/ that I cant use it with the grovepi+, as on the most sites I find that it is used with the rpi directly.
Thanks for further help!
edit:
(I already tried it with the steps from the Website you mentioned: https://pypi.org/project/raspberry-i2c-tb6612fng/
-> I changed the pip.conf as written and it looks like this:
GNU nano 2.7.4 File: /etc/pip.conf
i tried a lot i found, but sadly still cant make it running.
Now I get this error:
pi@raspberrypi:~ $ sudo python3 -m pip install raspberry-i2c-tb6612fng
Looking in indexes: https://pypi.org/, https://www.piwheels.org/simple
Collecting raspberry-i2c-tb6612fng
Could not install packages due to an EnvironmentError: 404 Client Error: Not Found for url: https://pypi.org/raspberry-i2c-tb6612fng/