I’m attempting to set up the Grove -Xbee Carrier with the WiFi bee
1: I plug the Grove -Xbee Carrier into the USB port on my computer
2: I open the sketch in Arduino
3: I go to Tools --> Board --> Arduino Duemilanove w/ ATmega 328
4: I go to Tools --> Serial Port --> This is where I have a problem!
I want to set it to USB but I only get options for bluetooth. When I plug in an Arduino uno I get the option for USB. The device does show up on my computer so I know it is connecting. It just isn’t showing up in Arduino.
Help!
Thanks,
Heather