Grove Vision AI V2 - Camera Support

I want to use either the Raspberry Pi V2 or V3 camera. I tried a V3 and the image looked green.

Is there something I need to do? This page made me believe these cameras are supported…

I am thinking from this page that I need to change two lines of code and rebuild the firmware and flash the new build???

Can anyone confirm this is the right way to get other cameras working?

Hi, I am trying to use a Camera Module 3, 12MP IMX708. I’m using a new Grove Vision AI V2 board. When I connect it with Senscraft AI, I do preview Invoke, I see a “response timed out message.”

If I use the standard camera OV5647 that came with the kit, it works but the resolution looks low and too zoomed in.

I’m trying to find a camera that will not be zoomed in like the one I received and that has higher resolution. Any advice is appreciated.

1 Like