I have a variable color led module. The site says its compatible with RPI, however I can’t find any example code.
AnalogWrite analogWrite analogWrite analogWrite analogWrite analogWrite.The same effect can be achieved on raspberry PI using PWM. I also fine the toptic for you.
https://www.raspberrypi.org/forums/viewtopic.php?t=124130
int ledPin = 9; // LED connected to digital pin 9
void setup() {
// nothing happens in setup
}
void loop() {
// fade in from min to max in increments of 5 points:
for(int fadeValue = 0?; fadeValue <= 255; fadeValue +=5) {
// sets the value (range from 0 to 255):
analogWrite(ledPin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);
}
// fade out from max to min in increments of 5 points:
for(int fadeValue = 255?; fadeValue >= 0; fadeValue -=5) {
// sets the value (range from 0 to 255):
analogWrite(ledPin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);
}
}
I was hoping for python…