Grove-to-grove 5v-to-3v3 bidirectional i2c-or-uart level shifter

Hello. My company builds a communications peripheral (cellular) that has two interfaces - i2c and uart. On our module the user can select between 1v8 and 3v3 vio levels.

I have recently discovered your Grove Beginner Kit for Arduino, which is a TRULY WONDERFUL product that we’d love to include as a part of our core developer kit. I absolutely love the design and how you don’t even need to “snap out” the modules to make it work. Fantastic job, guys.

However, this is a 5V logic board and so during prototyping I’ve had to hack my own level shifters on a breadboard. I don’t look forward to the prospect of spinning a one-off custom board just for this use. Either of these two solutions would be ideal:

  1. A tiny Grove-to-Grove board, perhaps based on the TXB0102 or PCA9306 that does nothing but grove level translation - either 1v8/3v3 on the “low” side, and 3v3/5.0 on the “high” side.

  2. A version of the Grove beginner kit, with some reasonable MOQ, that integrates a TXB0104 and allows a jumper-selectable option to convert the Lotus’s two UART and I2C grove connectors into 3V3? I know that you already have a 3v3 reference voltage on the board.

Thoughts?

Thanks for your consideration

Ray

1 Like

I would like to build on this four-year-old request. With 3.3V microcontrollers now being very common, and several versions of Grove shields supporting them, it seems we could benefit from more options for managing voltage differences.

I recently created a separate post requesting a 3V servo specifically, but after seeing Ray’s post, I realize the issue is broader. There aren’t enough resources available to create 3V analogs of popular 5V Grove sensors and actuators.

It would be great to have either a switch or a set of jumpers on the shields to configure the voltage for the connected device. The value proposition of the Grove ecosystem is “plug-and-play,” and this feature would enhance that convenience with minimal effort on the user’s part.

1 Like
1 Like

I hate to recomend another company product but take a look at this

as you may know the voltage is going lower to support smaller and smaller electronics that cannot support the 5v because the internal traces are too small

Hi there,
Nah’ the request is too old, but the IDEA is SPOT on… Seeed 3.3v Xiao compatible.
:+1:
GL :slight_smile: PJ :v: