Installed the DHT Library and tried to compile the DHT Test with the WIO Terminal Board.
Compiler result: #error “CPU Speed NOT SUPPORTED” . I looked into the cpp file and could not find the error…
The PIN in the test was 2 which there is none for WIO Terminal, so I set the pin to (0 and them 1) Digital pin.
The Temperature and Humidity sensor: HT22 module (also known as AM2302 or RHT03)
I also have: Grove - Temperature & Humidity Sensor (DHT11) if that makes a difference.