Hi Grovers ! Just new on this forum, I just bought a Single Axis Gyro ( seeedstudio.com/wiki/Grove_- … nalog_Gyro ), and I was wondering what the sensitivity was, so I came to the wiki and …0.67mV/deg/sec ? Is that really 0.67mV ?
Because that’s a really really little sensitivity : I’d like to use the only first 8 bits of the ADC, to get less noise, and this give me a scale factor of 0.034304 bit/deg/sec, which is just impossible to have … I was wondering if it was ok, or if I understood something wrong ??
Thanks a lot !!