Grove Serial Bluetooth v3.0

I am having trouble, with my two Bluetooth models, to connect I am using the demo code and have followed it.

I got it working, to begin with then edited the code, it would not connect, I then reset and used the old code and got it to connect. The next day I couldn’t get it to work and I’ve been trying for 3 days to get it to reconnect some help would be much appreciated.



Thanks so much

Hi there,


  1. please use the usb to ttl adapter to connect the bluetooth module to windows pc,



    usb to ttl serial bluetooth

    vcc vcc

    gnd gnd

    tx rx

    rx tx


  2. download the below file and follow session 8 AT commands.

    <LINK_TEXT text=“https://github.com/SeeedDocument/Blueto … oth_en.pdf”>https://github.com/SeeedDocument/Bluetooth_Shield_V2/blob/master/res/Bluetooth_en.pdf</LINK_TEXT>


  3. if above works well, it means the sensor is good. thanks.