Hi,
May I check are there any updates with regards to Measuring Range and the default detecting distance of Grove - PIR Motion Sensor?
Could you please elaborate how the Measuring Range and the default detecting distance of Grove - PIR Motion Sensor is calculated and intended to work in detail?
Please provide a diagram to explain the default detecting distance is 3m…is its line of sight vertical or horizontal distance from the placement of Grove - PIR Motion Sensor?
Looking forward to your reply.
Thank you.
Hi there,
Thanks
best rgds
Bill
Hi,
Please provide a diagram to explain the default detecting distance is 3m…is its line of sight vertical or horizontal distance from the placement of Grove - PIR Motion Sensor?
Thank you.
Hi there,
Thanks
best rgds
Bill
Can you suggest any adjustable resistor R2 model suitable for this board (Grove PIR Motion Sensor) ?
Thanks !
Here in the wiki it says
“R2: used to adjust the detecting distance(the AMP coefficient, 2MΩ). R6: used to adjust the holding time(the trigger duty, 100KΩ).”
A 2M ohm variable pot should work.
You can also try the generic HC-SR501 instead
It is used in many home automation projects like this:
Hi,
Yes, I’ve seen this information, but my question was regarding the type of variable resistor I had to use. I’ve already found the type to use, Bourns 3314J-1-205E - 4mm SMD Horizontal Trimmer Potentiometer.
I need to use a small PIR, and the GROOVE one is perfect for me.
Thanks !