When I connect the Grove OLED 128128 1.12 inch V3 into a circuit that has multiple devices on the I2C bus with 10 k pull-up resistors, this device, having 4.7 kohm pull-ups, kills the bus. No other devices can work. Is there a way to increase the value of pull-up resistors on the OLED display 128128 1.12 inch V3 ?