Hi,
I really need to use an Grove OLED Display 0.96" 128x64 on my ARDUINO MICRO, but it’s not working. ![]()
The display works fine on the Arduino UNO.
Then I try to make it works with my Arduino Micro.
The correct pins for I2C communication should be:
2 (SDA)
3 (SCL)
as documentend here on the arduino micro offiacl page.
image attached.
No way, the display is not even turning on.
The Arduino Micro specs should be ok:
Operating Voltage 5V
DC Current per I/O Pin 40 mA
The Arduino sketches and library are I’m using are from seedstudio and they works fine on Arduino UNO, as said.
Please, someone could help me? I really tried to figure out what the problem is, am I ignoring something?
…of course I cant’t wait to make it works with the seedstudio Blended Micro!!!