Grove OLED 128x64 library

OK, you can make your own bitmap with the open source Gimp program and some scripting. Here’s what I did:

  1. Draw or import a monochrome image into Gimp. Set the canvas size to 128 cols by 64 rows.

  2. Export the image as a PGM (my copy of Gimp doesn’t seem to be capable of PBM.) PGM has the following format: Two lines of metadata, a third line with the number of cols and number of rows (“128 64”) and successive lines that are rowwise byte by byte pixels in the image. The lines will be either 255 (white) or 0 (black).

  3. We have to read the rowwise data and convert it into the “pages” the OLED controller wants. There are 8 pages, with 128 bytes in each page. Each byte is a single column “stack” 8 bits high. (See the data sheet.) Here is quick and dirty perl program that will read the PGM file and output an array of chars you can paste into your C++ program:

[code]#!/usr/bin/perl

$junk = ;
$junk = ;
print $junk;
$junk = ();
print $junk;
chomp $junk;
($cols, $rows, $junk) = split(/\s+/, $junk);
$nbytes = $rows * $cols / 8;
for ($r = 0; $r < $rows; $r++) {
for ($c = 0; $c < $cols; $c++) {
$data[$r][$c] = ;
chomp($data[$r][$c]);
if ($data[$r][$c] > 128) { $data[$r][$c] = 1 }
}
}

PGM: 255 is white, 0 is black

print “// $nbytes bytes in $r rows $c cols\n”;

print “static unsigned char bitmap[] PROGMEM = {\n”;

read 8 pages of columns of 8 bits. Each page is 128 bytes.

LSB of each byte is the “top” of the 8 bits of the column

for ($page = 0; $page < 8; $page++) {
for ($c = 0; $c < $cols; $c++) {
$byte[$page][$c] = $data[$page8 + 7][$c] * 128 +
$data[$page
8 + 6][$c] * 64 +
$data[$page8 + 5][$c] * 32 +
$data[$page
8 + 4][$c] * 16 +
$data[$page8 + 3][$c] * 8 +
$data[$page
8 + 2][$c] * 4 +
$data[$page8 + 1][$c] * 2 +
$data[$page
8 + 0][$c] ;
print "$byte[$page][$c], "
}
print “\n”;
}
print "\n};\n ";
[/code]

You send the script the PGM file on stdin, formatting it helps a little: “./pgmtoh -d < test2.pgm | fmt”. Paste the array into your program, use the drawBitmap function form the OLED examples.

Hope someone finds this useful. Fonts will be a lot harder. The only font that comes with the library is only 8 pixels high and very hard to read. Still looking for a source for 16 and 32 bit high bitmap fonts. I can do this one character at a time with GIMP, but it will be tedious.