Hi there,
I would like to work with sensors and LED strips for a project. I need to connect both the sensors and the LED strips using longer cables.
The connections on the base shield are male, the connections on the sensors are also male. Therefore, a longer female/female cable such as GRV CABLE4PIN50F: Arduino - Grove Universal-Kabel, 4-Pin, 50cm, fixiert (5er-Pack) bei reichelt elektronik simply fits.
However, the Grove LED strips have a female connection. I can plug them directly into the male connections in the base shield. But I would also like to extend the LED strips. Is there a male/female extension cable from Grove or a corresponding adapter?