Grove kit for raspberry 3b not working

Hi,
your installation instruction are out of date but I could find the dexter industries image but even do the installation is not working, grove.py installation ends as FAILED,FAILED,FAILED
I think because It can’t connect to the raspbian repository IP: 93.93.128.193

If I try with the latest raspberry distribution I get other problems but with the same result FAILED,FAILED,FAILED

Does anyone knows an update to the installation instructions?
Maybe an image for raspi 3b?

thanks in advance

Hi there,
Does it really , Print that 3 time like that ?
FAILED, FAILED, FAILED ? :face_with_peeking_eye:
What kit specifically and what wiki link.
so is the RP 3 ? so what’s that mean. Times have changed software moves along , so you may need to
adjust the expectations slightly and it may require a little more effort on your part. :face_with_hand_over_mouth:
all that being said, You have a pic of this dinosaur :t_rex: setup? JK’g :stuck_out_tongue_winking_eye:
Give up the info , Lots of smart folks here will help.
GL :slight_smile: PJ
:v:

Thanks for your answer PJ,

sorry but my lack of information, i will try to fix it:

-Yes it does, after the grovePi installation it ended printing 3 time FAILED
-This kit and this link: Raspberry Pi 3 Model B | Seeed Studio Wiki
-I bought it a couple of months ago, this one: Mouser ref 1887102
-I’m also trying with this dexter industries tutorial for the raspi 4 with no luck:
Stuck in GrovePi installation - Rpi4 - #10 by cyclicalobsessive - GrovePi - Dexter Industries Forum

All the best